AXIS#.SENSORLESS.ISTART

Description

Sensorless Field-Oriented Control (SFOC) runs in open-loop when velocity is below a certain limit and automatically switches to closed loop when velocity goes above that limit. This limit is determined by AXIS#.SENSORLESS​.RPMSTART. There is a hysteresis band to make the transition seamless.

At open-loop, a constant current is applied to the motor to accelerate and reach AXIS#.SENSORLESS.RPMSTART. This constant current is determined by AXIS#.SENSORLESS.ISTART.


  • In the open-loop mode, AXIS#.SENSORLESS.ISTART value determines the maximum torque rather than the actual torque. The actual torque that is applied can be anywhere between 0 and this maximum torque depending on the load.

Versions

Action Version Notes
Implemented 02-03-03-000

 

General Information

Type

Read/Write

Description Sets the starting current for SFOC

Units

Arms

Range

0 to Drive’s Peak Current

Default Value

5% of Drive’s Peak Current

Data Type

Float
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
AXIS1.SENSORLESS.ISTART

5018h

05h

Signed32

-

1000:1

Read/Write

No

AXIS2.SENSORLESS.ISTART

5118h

05h

Signed32

-

1000:1

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.SENSORLESS.ISTART

7405

1CED

Signed32

Read/Write

-

AXIS2.SENSORLESS.ISTART

72941

11CE

Signed32

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.SENSORLESS.ISTART

7405

Float

Read/Write

-